CAP#.P

Description

The captured position. This value only changes when a new position is captured.

Examples

Usage

CAP#.SOURCE Description Units
1-5 FB#.P Same as FB#.P
11-12 AXIS#.PL.FB Same as AXIS#.PL.FB

Code

-->CAP1.P
0.000 [Counts]
-->

Context

For more information please refer to Capture.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read Only
Units

Depends on CAP#.SOURCE. See table above to know what the units are.

Range

N/A

Default Value 0
Data Type Float
See Also

CAP#.SOURCE, CAP#.T

Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

CAP1.P

31030

7936

Signed32

Read Only

Position

CAP2.P

31031

7937

Signed32

Read Only

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

CAP1.P

31030

Signed32

Read Only

Position

CAP2.P

31031

Signed32

Read Only

Position